Other Parts Discussed in Thread: XTR106
We are using the TI circuit that is shown in the TI datasheet. This circuit was used some time ago very successfully. Right now, the XTR106 has no 5V on Pin 14 and no 5.1V on the 5V Reg out pin. We installed a TI sample XTR106pa only on a board and 15V was connected to pins 10 and 6 and still no 5V. What is happening especially with the circuit? The circuit will indicate 4ma but when the sensor is pressured to 125psi the 4ma remains. Does the PN2222A enter into it? Mouser supplied the original parts.