I am trying to use the INA116 for high impedance measurements in a frequency range of 0.001 Hz to 10 kHz with the amplifier configured for G=1 (ultimately need to be able to handle 10V peak up to 10 kHz using +/-15V power supplies). The output of the INA116 is driving a 1 meter 50 ohm cable into the input of an EG&G 7260 Lock-In Amplifier which has a 10M ohm || 30 pF input. I am observing peaking at the output of the INA116 when being driven by a low impedance (50 ohm) sine wave at 1 V RMS (1.414V peak) starting at about 3 kHz but do not see the peaking at the guard outputs indicating an issue with the composite instrumentation amplifier. According to the datasheet this should be well below the full power bandwidth for the device (based on the slew rate that would be 18 kHz at 10V peak however this is only specified for G=10 to G=200 not for G=1). Below are some measurements at both 10 kHz and 100 kHz (I realize that at a G=1 there is peak of ~ 5 dB at ~ 500 kHz but is shown as flat to 100 kHz) - all inputs voltage levels are RMS:
@ 10 kHz
100 mV input 0dB peak
250 mV input 0dB peak
500 mV input 0.2dB peak
750 mV input 0.4 dB peak
1000 mV input 0.42 dB peak
@ 100 kHz
100 mV input 0.3dB peak
250 mV input 4.2dB peak
500 mV input 8.1 dB peak
750 mV input 6.1 dB peak
1000 mV input 3.7 dB peak - probably exceeds the SR of the INA116
Above measurements limited to 1V RMS due to LIA maximum input sensitivity.
I am less concerned with the 100 kHz measurements but the peak at 10 kHz is troubling (there is also about a 4 degree phase shift which exceeds the expected phase shift due to the 800 kHz G=1 bandwidth which should be about 0.7 degrees - ARCTAN [10/800]).
I have tried using the TINA 3 op-amp model provided by Matt Hann in an earlier post (since there is no SPICE model for the INA116) and do not see the peaking or phase shift issues (modeled the load as the 10 M ohm || 30 pF for the LIA input and a 100 pF shunt capacitance for the 1 meter cable. Is it possible that the amplifier does not like driving the cable capacitance and if so would a series output resistor be needed or helpful (datasheet lists amplifier Load Capacitance Stability as 1000 pF)? If that is not the issue Is there a way to compensate the amplifier to get flat amplitude and the expected phase due to bandwidth limiting at 10 kHz?
Any insight would be appreciated.
Don