Other Parts Discussed in Thread: THS3001
Hi,
I am building a simple three stage amplifier with the THS3001 with passive RC/CR filter in between each amplifier. I have the board running except that when I turn off the input I notice that the board is amplifying a strange signal at 3-5MHz. I've tracked down the problem to the power supply pins of the THS3001 which somehow has a signal of 5MHz going in. I also double checked the power supply and I am pretty sure the power supply is not the culprit. I currently have a 0.1uF cap connected to the power supply and ground. Is this the culprit? If so will adding a 6.8uF cap fix this problem? Thanks.