Hi,
I have to amplify a signal from order of nW to order of mW.
I tried to make rf by followeing TI's example with THS3202. (file name: RF and IF amplifiers with op amps)
I made the 40dB amp on prototype PCB by soldering and attatch THS3202 by silver paste.
But it has a parasitic oscillation.
Q1) What problem can be there?
So, I modified the circuit and made the 20dB amp. I think it is working.
Q2) If I make a few amp and connect them, I can make amlitude of signal from order of nW to order of mW?
Please quick answer.