Hello -
What is the input capacitance on the OPA693. Need this for the inverting and non-inverting inputs.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello -
What is the input capacitance on the OPA693. Need this for the inverting and non-inverting inputs.
Hello,
On page 3 of the OPA693 datasheet, the noninverting input impedance is given as 300kΩ || 1.2pF. The input capacitance is typically dominated by the package, so you can assume that the inverting capacitance is going to roughly equal to the non-inverting of 1.2pF. However, keep in mind that the inverting and output nodes are low impedance so any parasitic capacitance is going to have a negligible effect on the system response.
Regards,
Luke Lapointe
High Speed Amplifiers