Other Parts Discussed in Thread: LMH6505
hiall,
And AvMax=100V/V is usefull, see snosat4e.pdf and pabe 6 Fregaurecy
Rseponse for Various VG(AVMAV = 100) .
In a reference example, they are RF=2.32komega and RG=18ohm.
>RG=18ohm was not able to be chosen from Vin (MAX) regulation.
> 1) RG=180ohm from Vin(MAX) =0.9V.
> 2) AvMax = 100times it is RF=20komega.
Figure8 is 2.32komega f3dB=40 MHz.
From an inverse proportion rule, it is set to f3dB=4.64MHz by RF=20komega.
If there is no "feedback current to some extent, it will not operate normally." Although it is ,
How doesn't it operate?
Although it is not high bandwidth, may I think that it operates as 4 MHz of zones?
Regards,
Hisa Kobayashi.