This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Quad Op Amp Driving Capacitive load and fast Saturation recovery time

Other Parts Discussed in Thread: OPA4350, OPA4353

Hi

 

Could you recommend a quad op amp that can drive large capacitive load, and another op amp that has fast Saturation recovery time? It is ideally a 14SOIC package since I am trying to replace LMC660AIM (14SOIC package) on an existing board. Other quad op amp could be acceptable.

 

Thanks in advance.

 

  • Wen,

    With the very limited information you provided about the required op amp specifications (other than capacitive load drive and overload recovery time), I would direct you to take a closer look at OPA4350 or OPA4353 - they can drive directly capacitive load of 10uF or more while their typical overload recovery time is 100ns - see below.