Other Parts Discussed in Thread: THS4631
I am considering using THS4631 to sense an analog signal for a DSO (digital storage oscilloscope) application. The input signal will range from 0-500V with input frequency of 0-15MHz with the high amplitude signals (100V-500V) limited to 1MHz. This signal is input at the non-inverting terminal of the THS4631 through a 1M and 30pf parallel network. This network is between the CRO probe and the non-inverting terminal of THS4631, as the circuit will limit the input current flowing through the non-inverting terminal. Is it necessary to add protection diode at the non-inverting terminal? I would prefer not to do this as the reverse current will add noise into the circuit.