Problem:
*LM339 not switching when input voltages are close to each other(i.e. 2.62Vref on inverting ) and 2.8V on non-inverting input)
* Open collector output of the LM339 is pulled to +5V through a 10K resistor; When inverting input gets 187mV applied, with 2.8V present at non-inverting input , the LM399MX/NOPB operates as intended(i.e. open collector output gets pulled up-to +5V).
However, when Vref/inverting input = 2.62V, with the 2.8V still at +Vin, The LM399MX/NOPB output stays LOW. The IC does not seem to be discerning 180 – 200mV input difference.
Is there some internal hysteresis that we don’t know about…?
Digikey’s specifies the LM339MX/NOPB as a General purpose LOW power comparator type.
They also have the LM139AD which is of a Differential type.
I am confused as to what the difference (if any) is between a general purpose LM339 and a differential LM339.
I need the comparator’s output to float to +5V under both non-inverting input voltage (187mV & 2.62V) conditions.
Please advise on a viable alternative.
Thanks
Mamadee V. Fofana
Contract Embedded Systems Design/Development Engineer