I have a circuit with very high gain, 10 GOhm resistors. The photodiode has a very large cap. value 380 pf. I have compensation across the feedback resistor and I am using a OPA129 amplifier. When I put a step into the system there is a slight overshoot/ringing at the beginning and then a very long slow slope. The input signal has a time constant of 1us.
I was wondering if there where any suggestions for attacking this problem. We need the output to settle to < 0.5% within a second, the risetime looks fine, it is this low level ringing and drift that is the problem, on the order of 1%
Regards,
Jim Gannon