Other Parts Discussed in Thread: INA146, INA148, INA117
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: INA146, INA148, INA117
The INA146 CMV equation is 11*(V-) to [11(V+) - 1]....up to a maximum of +/-100. Split supplies of -5V and +15V would yield 11(-5) to (11*14): -55V to +100V.
If the customer needs up to 108 or 120V CMV, then I'd suggest the INA117 or INA148 that both go up to the +/-200V range. These however do not have G=0.1 options.
I'll follow up seperately with new developement ideas, but nothing short term to share.
Thanks,
niki