This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INA148: CMRR during run-time



Hi,

the CMRR is min. 70dB, the typical value is 86dB. The customer is doing calculation for the system and is measuring the exact CMRR for the devices. Is this measured CMRR constant during the run-time of 10 years. Or is this a constant value means the measured CMRR (e.g. 80dB) is constant?

BR & thanks a lot, Xaver