Other Parts Discussed in Thread: THS4524, THS4522, ADS1278, THS4521
I am designing an audio system and am looking for an amplifier to drive the differential inputs on my 4-ch, 24-bit audio ADC. The specifications I am most interested in on the ADC are dynamic range of 115dB, THD+N of -102dB, and channel separation of 120dB. The system has a tight power budget, so low power is essential. Does TI have an input amplifier for my application?