Other Parts Discussed in Thread: INA196
Sorry for my lack of experience with these but I have a situation where the INA196 is being damaged. I haven't been able to observe the fail but I suspect transients due to switching between two power sources that are monitored by this device. The INA196 is measuring across a 1 ohm resistor in series with a load and is supplied by switching between one of two batteries. The battery input is less than about 32V and the load is a DC to DC power supply and the grounds are all connected. The currents will be about 0.5A or less. The datasheet indicates to add zeners or transzorbs to the input but I'm unsure how they should be connected. I'm thinking about opposing zeners connected to Vin+ to ground to protect + and - voltages, the positive protection zener is 39V and the negative oriented zener is 12V. I'm worried that this configuration would expose the zeners to too much current and they too will fail. Any advice is welcome.