Other Parts Discussed in Thread: THS5661A, OPA2822
Customer is looking at using the OPA2822 configured as a current divider between a current output DAC (THS5661A) and their analog ASIC. Their ASIC input is an amplifier and is very sensitive to capacitance on the input. They want to know what the output capacitance of the OPA2822 (including package) would be. DAC can be clocked as high as 48 MHz.
Op amp circuit:
ASIC input (output load for op amp circuit)