Other Parts Discussed in Thread: INA321
Hi,
first post so forgive me any lapses in etiquette!
I see in the datasheet for the INA321that pulling the shutdown pin to 0V puts the device into shutdown mode and that the output impedance then goes high and therefore suitable for multiplexing..
I was thinking of using a 3 t0 8 line decoder to select which one of 8 INA321s to read...
My problem is that I don't have access to the shutdown pin as the amplifiers is located at the end of 3 core cables, next to their respective strain gauges.
can I get the outputs of the 7 devices to go high impedance and therefore suitable for a input to a single DA convertor by using the decoder to connect VDD or VSS to the INA321 instead of using the shutdown?
Chris