Other Parts Discussed in Thread: XTR117, XTR111, ISO1541, DAC7571, DAC7311
Hi,
Customer is going with the XTR117 (2 wire solution) (over the XTR111) and is looking at doing the PWM option like they are showing on page 7 of this datasheet.
In the end they would like to meet or exceed the 12 bit resolution they have today using a DAC and the update rate needs to be 3KHz min.
“I would also like to use the Vreg output as the supply for the isolation...
The trouble I'm having is again at that update rate (3KHz) and ~12 bit resolution on the PWM I need a ~100MHz isolator which requires more current then what can be supplied from the XTR
Does TI have any recommendations for the XTR117 for 3KHz update, small, cheap and uses the Vreg output to power isolation?”
Customer looking at the ISO1541 for isolation.
Any suggestions would be appreciated!
Thanks,
Adam Hoover
ACAT Support