This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WILL LM1881N PRODUCE VERTICAL SYNC OUTPUT WITH ONLY VERTICAL SYNC AS INPUT INSTEAD OF COMPOSITE VIDEO?



I was using the LM1881N to receive SD composite video and output vertical sync pulse to my equipment.

The equipment needs the vertical sync to function.

I'm switching to a HD video camera which has no composite output.

The new camera has a veritical sync output but I can't connect directly to the equipment, there needs to be a buffer.

If I feed just vertical sync to the chip will it still put out a vertical sync and act as a buffer? If not is there another chip which will work as a buffer?