Other Parts Discussed in Thread: THS4521, TINA-TI
Hello,
I am currently working on an integrator device using a THS4521 amplifier in a differential input/output configuration.
The amplifier is powered with 0/+3,3V supply and an offset of 1.65V. (see attached files)
Despite Tina-Ti gave simulation results I expected, real experiment shows that the amplifier is unstable for an offset range from 0 to 2.8V (signal oscillations). Expected characteristics are obtained when offset>2.8V.
Do you have an idea of the origin this instability problem? The problem still occurs when I remove load capacitors or decrease the closed-loop gain.
Regards,