Other Parts Discussed in Thread: OPA3693
Hi,
Could you please tell us the Absolute Maximum Rating of OPA3693 OUT pin and DIS pin ?
Best Regards,
Kawai
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Kawai,
Sorry for the delay in reply. The Absolute Maximum Rating of OPA3693 OUT pin and DIS pin is not defined in the datasheet. However, the limits are set through characterization, the OUT pin could be DC coupled and hence should be good within 0.5V of the supply. But, distortion would be worse when operating the output common mode at near the supply rails. Same for the DIS pin maximum should be good enough to upto the supply voltage with atleast 3.7V for the amplifier to be enabled.
Regards,
Rohit