Other Parts Discussed in Thread: LMP8358
Hi,
I'm using the LMP8358 in a strain gauge application. So far, the normal mode with gain = 1000 work very good. In order to detect possible error in the strain gauge, I'm using the suggested error detection methods (short, open connections etc.) described in the datasheet.
However, there is some strange behaviour. In any case I don't use the internal current source, switching between the error modes is very fast. In case I use the internal current source (to detect a open connection), it will take about 100µs after the rising edge of CS until the output starts to change to the correct voltage level. Additionally, there is a 200µs settling time in this case. In comparision, switching from a non current source mode to normal takes less than 20µs.
I cannot find anything about this in the datasheet, so is this a desired behaviour? OR am I missing something?
Cheers
Stampede