Other Parts Discussed in Thread: ISO122
Hello,
I am using eight ISO122U Isolation Amplifiers in my desing, placed on the bottom side of the PCB (placement area is about 40 x 50mm).
Supply voltage is +/-15V on input and output side.
I'm using them to transfer a slow 0...10V signal (max. 1kHz).
Problem: The ISO122U get very hot, they reach >70°C and heat up the PCB (and the components on the top side).
I cannot imagine that this is normal, although the power consumption at 15V is relatively high (ca. 0,6W according to datasheet).
Is there anything I can do? My first try was to reduce the supply voltage at the output side from 15V to 12V, but that helped only a little bit (temp. >=65°C).
What else can I do?
Kind Regards,
Michael