Other Parts Discussed in Thread: ADS6445, THS4508, THS4509, THS4511, THS4513
I have to design an analog interface to the ADS6445 (quad, 14-bit, 125MSPS ADC). Below are the requirements that I have to meet: 1. DC coupled 2. Single supply 3. Bandwidth = 0Hz to 250MHz ideally but at least 0Hz to150 MHz. 4. Vocm = 1.5 V Could you suggest a part suitable for this application?