Hi
I would like to make a 100mA, 100ns current pulse (or somewhere in this range and a bit below, maybe 50mA 100ns is OK) to a small capacitor to test its ESR accurately.
I understand that I cannot use a function generator to do this and I need to use some kind of amplifier circuit. There are voltage controlled current source examples in a few datasheets
http://www.ti.com/lit/ds/symlink/ina128.pdf
http://www.ti.com/lit/ds/symlink/ina114.pdf
This style has also been presented elsewhere outside of TI.
However these are using amplifiers with slew rates of below 10V/us. There is no way they can make the 100ns current pulse I need?
Would I use similar designs to this and simply select faster opamps? However in simulation it seems that if the opamps are too fast then this also causes problems...
I am not familiar with selecting opamps and I can see that generating repeatable current pulses of this magnitude does not appear to be trivial
Any help appreciated