Other Parts Discussed in Thread: LM675, TINA-TI, OPA541, OPA549, LM1875, LM3886
Many amplifiers need split power supplies to produce AC wave forms. When all you have available is a single DC source there are a few ways to fabricate an inverted source and virtual ground. I have tried a few of these schematics by building them in Tina-TI, and remarkably most do not work. Even the one on the LM675 datasheet (figure 3) does not work in Tina-TI when built exactly verbatim.
The chip based versions are usually limited to 500mA but I need 5A. Can someone suggest a schematic that will absolutely work to provide +/-20V from a 48V source?