This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

how to provide 250 VAC protection on precision current source output



In instrumentation requirement I need to provide 250 VAC protection on the precision current source.  Can any one suggest how to do it.

  • Hello Madhusudan,

    I am not certain the exact sort of protection your application requires. But if it is one where the voltage needs to be clamped if it exceeds 250 V peak, then a transient voltage suppressor (TVS) diode may be applicable. You can view information about TVS diodes on the Littelfuse website:

    http://www.littelfuse.com/products/tvs-diodes.aspx

    They offer a variety of over-voltage protection devices. Other manufacturers provide similar products.

    Do review the TVS device specifications to make sure the leakage current, capacitance, etc, are compatible with your precision current source circuit.

    Regards, Thomas

    PA - Linear Applications Engineering

  • Dear Mr. Thomas,

    Here with I am attaching the output stage diagram for which output shall be protected from accidental shortcircuits to the 240 VAC lines.  The circuit diagram was sent to you thru separate email.

    Kindly let me know , how can i attach a pdf file to this post?

    regards,

    B. Madhusudan

  • Hi Madhusudan,

    I don't think that a pdf can be directly attached. I usually copy the selected image into Micrsoft Paint and save it with the .png or .tif extensions, or Zip the pdf and then attach it. You select the Options tab shown above to attach the file.

    Did you send the schematic to my email address? I am not seeing it. My email address is:

    kuehl_tom@ti.com

    Regards, Thomas

    PA - Linear Applications Engineering