I have designed a biomedical device around xtr111. Everything is fine, and working as expected and reported in the data sheet. However EF pin showed a strange behaviour. When the supply voltage is >15V, then EF does not toggle when output current is disconnected (flows through 1meg resistor, but not equal to 2mA that was set). Following is the relevant and the only description from data sheet. I think it is missing a deeper detail.
Regards,
Adnan
"The XTR111 has additional internal circuitry to detect The input voltage range for a given output current an error in the output current. In case the controlled span is set by RSET according to the transfer function. output current cannot flow due to a wire break, high Select a precise and low drift resistor for best load resistance or the output voltage level performance, because resistor drift directly converts approaching the positive supply, the error flag (EF), into drift of the output current. Careful layout must an open drain logic output, pulls low. When used, this also minimize any series resistance with RSET and the digital output requires external pull-up to logic high VIN reference point. (the internal pull-up current is 2μA)"