Other Parts Discussed in Thread: INA194, INA210, INA213
I have five high side inductive current monitor circuits each driving hydraulic solenoids. The INA194 is used to measure the current and the inductive flyback. The specs are: 0.62 ohms sense resistor, Vs = +5V. When the high side FET driver is off the common mode voltage to the INA194 is zero. Under this condition I normally measure 0.008 volts to 0.030 volts as the offset error due to common mode voltage being lower than Vs. On the last lot of production assy's, I have measured 0.116 to 0.123 volts on specific devices. The devices in question is replaced and now in spec. If I energize the high side driver to raise the CM voltage to +12V and Vdif = 0, the offset voltage will drop by half. What is happening and any solution?
Regards, R.Engholm