Other Parts Discussed in Thread: ISO122
Hello,
Please advice ISO122 power-up sequence restriction of –Vs1, +Vs1, -Vs2 and +Vs2.
Regards.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: ISO122
Hello,
Please advice ISO122 power-up sequence restriction of –Vs1, +Vs1, -Vs2 and +Vs2.
Regards.
Ushikubo-san,
The intended power-up cycle for the ISO122 is the same as it is for nearly all analog integrated circuits; they are intended to have all supplies - positive and negative - brought up simultaneously. That is the way they are powered on and off during internal test and characterization. No special characterization evaluating different power supply sequencing is done.
Regards, Thomas
PA - Linear Applications Engineering
Hello Tomas-san,
Thank you for your answer.
Please answer additional question.
< Q1 >
Are there any power-up restriction between Vs1 and Vs2 ?
< Q2 >
Customer plan to supply “15V +/-5%” to +Vs1/+Vs2 and “-15V +/-5%” to –Vs1/-Vs2.
Please advice if above tolerance between + and – power supply is OK.
Best Regards.
Ushikubo-san,
The normal ISO122 power sequence has all of the supplies, +Vs1, -Vs1, +Vs2, -Vs2 powered up, or down, at the same time. No formal characterization of other power sequences has been done. Although no damage has been reported when customer's have brought +Vs1/-Vs1 before +Vs2/-Vs2, or visa versa, the output behavior during such power sequences has not be characterized and cannot be assured.
The customer's plan to employ 15V +/-5%” to +Vs1/+Vs2 and “-15V +/-5%” to –Vs1/-Vs2 is very good.
Regards, Thomas
PA - Linear Applications Engineering