on page 9, we can see two graph small and large signal pulse response.
is the dv/dt correct?
is the slew rate 4v/10us?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
on page 9, we can see two graph small and large signal pulse response.
is the dv/dt correct?
is the slew rate 4v/10us?
The slew rate is better than that and is typically measured between 10% to 90%. Eyeballing the graph this looks better than 5us, which is in line with the slew rate spec of 1V/us.
The output settling time to 1% final value, on the other hand, is specified as 20us typical. This may be what you are referring to. In the graphs the signal seems to settle around that value.
Regards,
Sergio