Hello all,
I'm experiencing some rather unusual fault behavior with the THS4032CDGN op-amp. My design uses op-amp in a split-supply application, with dual LM2596-ADJ buck regulators converting 24V input to a +-15V supply. The circuit is assembled using SMDs on a PCB. The power supply operates properly with no other components installed, drawing about 70 mA @ 24V quiescent current.
When I install the op-amp U1 (see the schematic below), with no other components installed, my 24V power supply collapses to about 2V @ 2.2A. The negative buck regulator outputs -3V, while the positive regulator outputs -200mV. The negative regulator becomes hot to the touch; other ICs do not. The op-amp outputs and inverting inputs show DC voltages ranging from -0.5V to -2V.
Next I removed U1 and installed U2, again with no other components installed. The circuit pulls between 100-110mA @ 24V, meaning U2 is responsible for about 30-40mA current draw. The +-15V supply operates normally. U2 quickly becomes hot to the touch. U2A outputs -12.8V (sticks to negative rail), while U2B outputs zero volts.
I repeated this procedure on another PCB and got the same (unwanted) results. The PCB is not faulted; I probed all the tracks and found no short-circuits. Can anybody offer some insight into this peculiar behavior? It's very difficult to solder the thermal pad underneath the DGN package. Am I perhaps frying the op-amps during hand-soldering?