I am feeding multiple sensors into a multiplexed ADC.
One sensor has a differential output and is being fed into an INA128 chip and amplified with a gain of 150 (using 333ohms). This amplifies the original value to somewhere less than 2Volts and I'm happy with that behavior.
The other sensor has a single ended output of 0 to 10 volts. I am feeding this sensor through it's own INA128 so that the two sensors will have a common ground. If I don't feed the 10v sensor through an INA128, it's floating ground causes the other sensor's output to mimic the 10v sensor's output (interference).
So far I am successful in routing both sensors through their own INA128s and knocking out the interference from one sensor to the other.
Here's the question... The 0 to 10v sensor saturates it's INA128 so that the output only reads around 8.5 volts when it should be reading 10 volts. The gain is set to zero (no resistor and no amplification) and the supply voltage is around 24 volts. When the supply voltage is only 5, the saturation point is much lower (something like 2 or 3 volts out when it should be 10). What would I have to increase the supply voltage to the INA128 to in order to see a direct 1-to-1 maximum 10 volt value from the sensor and 10 volt out of the INA128 ?
Also, the data sheet seems to say that the max supply voltage is +/- 18 volts, whereas the web site seems to say 36 volts max for supply voltage. (is the range of -18 to +18 being 36volts the reason for the web site saying 36 volts?)
If I get a DC/DC converter with 36volts for the supply of the INA128 would I be able to see the 10 volts from the sensor make it all the way through the INA128?
Thanks in advance,
Chris