Other Parts Discussed in Thread: LMH6554, LMH6552
Hi,
our ADC output a voltage to feed ADC Driver VCM.
We would like to understand what is the Impedance on the common mode pin in a few scenarious.
The questions should regard to all the LMH series
For the LMH series of TI ADC drivers, I would like ask the following :
- What is the VCM to GND impedance while the LMH IC is not powered.
As we intend to work with negative voltage, that means V+ and V- pins are floating as well as VEN
2. What is the VCM to GND impedance while the LMH is powered on but disabled using VEN
This means : V+=+5V, V-=-5V, VEN<0V so that the IC is in disable mode.
Thanks.