Other Parts Discussed in Thread: LMC6001, LMP7721, LMC6081
We have been trying out the LMC6001AIN in a transimpedance amplifier that uses a 100G feedback resistor. What we find is that after a current input of 0.1nA is disconnected, the output does not return to its baseline in the way we would expect. The output drops to about 50ppm of the full scale value in a time consistent with the circuit's frequency response (1.6Hz), i.e. 2 seconds, but then has a slow decay back to the baseline over many tens of seconds.
We believe we have followed good practice relevent to low currrent measurements in the design of this amplifier. We have taken heed of the article "Design femptoamperecircuits with low leakage" published in EDN by Paul Grohe.
The curious thing is if we replace a LMC6001AIN currently manufactured by Texas with a metal canned LMC6001AIH manufactured by National Semiconductor, the recovery time is much better. The output drops below 25ppm of full scale in 2 seconds. This difference is important to us and we would like to use the LMC6001AIH, but Texas doesn't make them! The difference is repeatable with several samples of ICs from different batches.
What causes this final slow decay? The negative input is at virtual ground, so it is difficult to believe it is charge storage. Also what causes the difference in behaviour between the two parts? is it the difference in package, or have other changes taken place in the design of this chip since the metal package was made obsolete?