Other Parts Discussed in Thread: THS3001
Hello to everyone, we are having several problems using THS3001 and we were wondering if we could have some help.
The schematic below ilustrates our circuit, a simple non-inverting amplifier with the next considerations:
- Gain: ~ 80 V/V.
- Minimum required BW: 20 MHz approx.
- Input signal amplitude range: 0-30Vpp.
- Because of application restrictions it is not possible to limitate input voltage nor including any resistor at the input.
The amplifier operates very good while it is not saturated and have a regular temperature of ~ 40ºC. Problems come when the amplifier starts saturating (with ~300 mVpp at the input), at this moment it starts to get very hot (70-80ºC) and finally breaks even with low frequencies (500kHz). Notice that the application requires that it must support up to 30Vpp at the input, although it is saturated most of the time.
We've tried to increase the feedback resistor as much as we can (up to1k) to reduce the output current as much as we can but the problem persists. THS3001 datasheet specifies that the amplifier resists an input of +- Vsupply, then ¿why do we have this problem?¿Any idea or solution?