Other Parts Discussed in Thread: AFE031
hi, i'm trying to comunicate with an AFE031, i would like to understand how receive data from the spi, if i need a cycle of reading after one of sending data.
here is the code i wrote:
#include "inc/hw_types.h"
#include "inc/hw_gpio.h"
#include "inc/hw_ints.h"
#include "inc/hw_memmap.h"
#include "driverlib/sysctl.h"
#include "driverlib/interrupt.h"
#include "driverlib/rom_map.h"
#include "driverlib/gpio.h"
#include "driverlib/timer.h"
#include "driverlib/ssi.h"
#include "driverlib/pin_map.h"
#include "utils/uartstdio.h"
#include "driverlib/uart.h"
#define PINDAC GPIO_PORTA_BASE,GPIO_PIN_6
unsigned long DataRx[1];
void ConfigureUART(void);
int main(void) {
SysCtlClockSet(
SYSCTL_SYSDIV_5 | SYSCTL_USE_PLL | SYSCTL_XTAL_16MHZ
| SYSCTL_OSC_MAIN); // Clock setting
MAP_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA); //Abilita la porta A
MAP_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOF);
SysCtlPeripheralEnable(SYSCTL_PERIPH_SSI0); //Abilita periferica SSI0
ConfigureUART();
GPIOPinConfigure(GPIO_PA4_SSI0RX);
GPIOPinTypeSSI(GPIO_PORTA_BASE, GPIO_PIN_4);
GPIOPinConfigure(GPIO_PA3_SSI0FSS);
GPIOPinTypeSSI(GPIO_PORTA_BASE, GPIO_PIN_3);
GPIOPinConfigure(GPIO_PA2_SSI0CLK);
GPIOPinTypeSSI(GPIO_PORTA_BASE, GPIO_PIN_2);
GPIOPinConfigure(GPIO_PA5_SSI0TX);
GPIOPinTypeSSI(GPIO_PORTA_BASE, GPIO_PIN_5);
SSIConfigSetExpClk(SSI0_BASE, SysCtlClockGet(), SSI_FRF_MOTO_MODE_0,
SSI_MODE_MASTER, 10000, 16);
SSIEnable(SSI0_BASE);
GPIOPinTypeGPIOOutput(PINDAC);
unsigned long rxdata;
UARTprintf("test\n");
SSIDataPut(SSI0_BASE, 0x8200);
SysCtlDelay(13333);
SSIDataGet(SSI0_BASE, &DataRx[0]);
SSIDataPut(SSI0_BASE, 0x0000);
SSIDataGet(SSI0_BASE, &DataRx[0]);
while (SSIBusy(SSI0_BASE))
;
UARTprintf("DieRev: %X\n", DataRx[0]);
// SSIDataPut(SSI0_BASE, 0x8A00);
// while (SSIBusy(SSI0_BASE))
// ;
// SSIDataGet(SSI0_BASE, &DataRx[0]);
// UARTprintf("DieRev: %X\n", DataRx[0]);
while (1) {
}
}
void ConfigureUART(void) {
//
// Enable the GPIO Peripheral used by the UART.
//
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA);
//
// Enable UART0
//
SysCtlPeripheralEnable(SYSCTL_PERIPH_UART0);
//
// Configure GPIO Pins for UART mode.
//
GPIOPinConfigure(GPIO_PA0_U0RX);
GPIOPinConfigure(GPIO_PA1_U0TX);
GPIOPinTypeUART(GPIO_PORTA_BASE, GPIO_PIN_0 | GPIO_PIN_1);
//
// Use the internal 16MHz oscillator as the UART clock source.
//
UARTClockSourceSet(UART0_BASE, UART_CLOCK_PIOSC);
//
// Initialize the UART for console I/O.
//
UARTStdioConfig(0, 115200, 16000000);
//
UARTStdioConfig(0, 115200, 16000000);
}
thanks