Please refer the connections of INA326 which I did in circuit. Initially I have assembled this much circuit only to check the performance of INA 326 and it is working fine.
Now I have integrated power supply sections(IC- TPS 5430 and IC- LM 2830) and 4-20 mA section(IC- XTR 111) along with this INA 326. All sections are working fine except INA 326.
I have Gas sensor whose operating voltage is 2.4V. So my common mode voltage becomes 1.2V. The input signal to INA 326 is around 120-160mV and I have to amplify it over 0-5V range.
The reference input of INA 326 is adjusted by potentiometer(1k).When both the input terminals are at same potential, the output should be zero ideally (practically 50-60mV). But I am getting around 600 to 700 mV output when the bridge is balanced and that output voltage is not changing as expected after unbalancing the bridge (by applying gas to gas sensor). There is very small change in output voltage.
Kindly advise
Atul Bhakay
Please advice with your suggestions.4064.INA 326.pdf