Other Parts Discussed in Thread: TLE2141, OPA378
I have a customer who is using the TLE2141 in one of his designs, but the the Spice model does not have the pin designation for the offset pin.Customer is intending on using the TLE2141 in a 0-30VDC variable Power Supply with adjustable current and is trying to simulate the circuit but the Spice models did not contain the offset pins. The way his circuit is configured,these pins allow for the adjustment for the voltage output to reach 0V nomatter the tolerances of the rest of the components. Is there a way toaccomplish this or is there a more suitable model he can use? Aslo I checkedthe datasheet for this device and on page 2 it says that the offset optionis available only on TLE2241x device, is this a typo?