Other Parts Discussed in Thread: OPA4350, OPA4353
Could you give me a few recommendations for the amplifier with large capacitive load driving capability? I would want a quad opamp with 16 pin SOIC package; and Vs is +/-5V. Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Huang,
A "large" capacitive load is a relative term - you need to be more specific. Are you talking about few nano or micro-farad?
The only op amp I know that can directly drive several uF capacitive load is OPA4350 but it is 5V (or +/-2.5V) and not 10V supply part you asked for. You can improve the capacitive load drive of any op amp by adding a small (10ohm to 50ohm) series output resistor but this may create a gain error if your application involves a resistive load.
To get around this problem, a dual feedback configuration shown below will dramatically improve the capacitive load drive of any op amps at the price of significant decrease of its effective bandwidth.
Thanks for the reply.
Wen,
OPA4353 is an untrimmed version of OPA4350 which I previously suggested for driving high capacitive loads but I have no comparable part to suggest for 10V supply. If you have no resistive loading, you may just need to add a series output resistance to improve the capacitive load capability of any op amp; otherwise, you may have to implement the dual feedback solution shown in my previous post.