Hello,
I am using LM2904QDRQ1 in an application as a current sense amplifier.
I have a few queries:
a) The datasheet specifies the values of input offset voltage, bias current and offset current as follows:
Here, the minimum values (MIN) are not specified.
Could you please provide those values?
b) The input bias current values are specified as negative.
While doing analysis do I need to consider both positive and negative polarities?
c) Below is the circuit attached for reference and the equation used for output voltage.
Please see through and suggest if this is correct or needs to be updated:
Here,
Vout : output voltage of Opamp,
I.sense: current across resistor R4,
Vos; Input offset voltage,
IB: Input bias current,
Ios: Input offset current
R4: sense resistor
R1, R2; series resistors
R3; feedback resistor
Thanks a lot for your support.
Regards,
Swati Jain