Other Parts Discussed in Thread: OPA27
I am trying to use the OPA633 buffer to replace Intersil HA3-5002-5Z
which is now obsolete. Our product has been in production some time, and we do
not want to re-design it yet. The OPA633 is the only device that I can find that
is almost pin compatible with the old part. The application simply uses the OPA633 to buffer the output of a standard OPA27
op-amp to give a higher current drive. It is included into the feedback loop of
the op-amp in a way that is very similar to the application examples fig.3 and
fig.4 on the device data sheet. The power rails are +/-15V. My problem is that
the OPA633 runs very hot at all times, even when there is no load on the output
and the o/p is just static at zero volts DC. Even when loaded I only expect to
load the output to maybe 50mA. The package temperature quicky rises to over 40
deg C in free air. Am I doing something wrong? I was not expecting to need a
heat sink (difficult with a DIP8 package). I have tried different ICs from
different batches, so I know it is a design issue and not just a defective
chip. Can anyone suggest a cause?