Other Parts Discussed in Thread: OPA2364, OPA2314, OPA364
Hi,
I need a differential output AC constant current source of around 100 or 200mA. Freq is around 20 Hz.
Can I build that using a pair of Howland Current pump ?
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Siauhwa,
Yes, two Improved Howland Current Pumps can be used to generate differential ac currents. The key to making this straightforward and accurate is to drive the two pumps from the same differential output voltage source. Either an operational amplifier having a differential output, or a dual operational amplifier configured as a single-ended input, differential output amplifier.
I have attached a slide created by one of my colleagues showing how to create the single-ended input, differential output amplifier. An OPA364 (OPA2364 is the dual) is shown in the schematic. Since your application doesn't require speed a lower current amplifier such as the OPA2314 would be a good choice to reduce power.
Regards, Thomas
PA- Linear Applications Engineering
Hi Thomas,
I'll try it and I'll let you know ...
By the way, do you have the TINA simulation/result for that circuit ?
Thanks
Hi Siauhwa,
You can try clicking on the TINA symbol shown on the slide. I think the TINA file for the single-ended input, differential output amplifier is embedded - at least it opens directly from TINA when accessed from my original slide.
However, if that doesn't work I've attached a TINA file for the circuit.
Regards, Thomas
PA - Linear Applications Engineering