What is the 1% settling time of the THS7530 to a 10 or 20dB gain step. Not the amplifier settling time-- the settling time due to a gain step.
The data sheet doesn't seem to address this although the gain control BW is spec'ed as 15MHz.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
What is the 1% settling time of the THS7530 to a 10 or 20dB gain step. Not the amplifier settling time-- the settling time due to a gain step.
The data sheet doesn't seem to address this although the gain control BW is spec'ed as 15MHz.
Hi Neil,
You are correct there is no information on that parameter in the datasheet. They also list the 15MHz as "small signal" bandwidth for the gain control circuit.
At 38dB/ volt the 10dB step is pretty small at 0.25V, but the 20dB step is ~0.5V which is half of the total range and I doubt that falls under small signal conditions.
What settling time does your application require? Have you tried the model in TINA?
Regards,
Loren
Thank you for your reply, Loren.
Yes, I simulated a small gain step in TINA and it shows a Tr & Tf of about 1.25ns. It would be nice if it could actually do this... but I fear this is a result of yet another poor TI device model. This is a key parameter for a VGA...who is the product line manager?
I need a step response 1% settling time of 150ns maximum.
Thanks, Neil ex-BB