Other Parts Discussed in Thread: LOG114, LOG112
Hello,
I'm using the log 112 as a current sensor. I set I2 to 70.7nA as the reference current, and my input current I1 varies between 100pA and 50uA. I'm finding that I need a compensation capacitor Cc of at least a 4.7nF to achieve a linear response at very small input currents, and this value capacitor causes the response time to be far too slow (I need less than a 4ms response time for changes of about a decade). The bandwidths listed on the datasheet of the log114 seem much higher, though it is for a much larger reference current (1uA). There also isn't an external compensation capacitor for the log114. Is the log114 a faster part, that might help solve my problem?
Thanks,
Lucy