This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

low input bias current Op-amp for accelerometers' charge amplifier



Dear experts,

I am designing charge amplifier cuicuit to convert charge to voltage output for accelerometers' aquisition circuit.

Sensitivity of the charge amplifier is 10pc/g. I want a sensitivity of 100mV/g. The mission profile is 150degreeC. REF_SHK is 2.5V.

I designed the circuit like this:

Do you have any concern about the circuit?

Op-amp for the first stage should be low input bias current op-amp. How low should the input bias current be so that it won't affect accuracy of the circuit?

Do you have any suggstions about which op-amp should I use?

Thank you very much and have a nice day!

Best Regards,

Xiaoxiao