Other Parts Discussed in Thread: PGA309EVM-USB, PGA309
I used PGA309EVM-USB board in my application, the software is sboc320c
I found something wrong but i can't find out it.The issue:
I compensate the PGA309 with 3 temperature point -40,0,60. the Temp ADC may be 0xFF60, 0x0000,0x0078
the temperature reg6 set as 1600,9-Bit + Sign, Right-Justified, Sign-Extended, Twos Complement,0.5°C (3ms)
just you can see from the E2PROM picture below
but when I finish the compensate , the E2PROM value just like this just like the picture below
the T1 ~T5 are 0x0000, the T6 is 0x 003 and the T6 to T16 is increasing but I can't find the FF60 and can't find the temperature below 0, what had happened when during wite the E2PROM,I doubt any bug in 320C software?