Customer is designing low current / speed light sensitive diode product using the TLV2410 as very low current TIA for 3VDC long life battery operation (> 7 years).
Candidate circuits (attached a TINA schematic entries ... not as actual simulation attempts) show initial design (diagram 1) with equivalent idle operation (as diagram 2). Actual operation draws 10x the datasheet current indicated (around 10uA vs. ~1uA). Note the operation is single supply 3VDC with a switchable offset voltage at the plus input of ~200mV (not the Vcc/2 on the datasheet).
Circuit in digram 3 shows a circuit which approached the datasheet current, but required an undesired bias idle current of 1uA (compared to 0.7uA opamp draw).
Questions are:
1. What mechanism is causing the 10x current draw in the TLV2401 for this circuit (are there additional test plots available indicating a change in current draw vs. input voltage)?
2. Why does circuit in diagram 3 cause the datasheet spec'd current draw (for 3k feedback resistor) but much higher draw for a 300k feedback resistor?
3. What recommendations / circuit configurations could be made to allow for a low current draw circuit for this application (target is ~1uA total ... including bias)?
The atttached TINA schematics include additional explanatory notes.
Thanks,
Phil