Hi,
I am using the VCA2615 as an Rx amplifier in my system. The input signal level is few microvolts and it is a differential signal.
Apparently, is seems as if the noise level (even in the EVB) is around few 00s of microvolts. This makse it difficult for us to interpret the signal we are looking for.
Signal frequency: ~1MHz
In order to amplify the signal, the following path is used:
input_signal --> filter--> LNA_A --> VCA_A --> filter --> LNA_B --> VCA_B --> ADC
The filter is a single pole LPF, set at around 1MHz.
Please advise on the following:
1. What is the CMRR and PSRR of the VCA2615?
2. Is there a problem with cascading the 2 channels of the VCA2615?
3. Is there an amplifier that is designed for 10uV input signal level, which will fit my design more than the VCA2615?
Thanks,
Avishai