Other Parts Discussed in Thread: DRV135
Hi Sir,
We are using Line driver DRV135 in one of our design. We are sending sine wave of 2.5V amplitude to the driver. When we probe at input to line driver there is no DC offset. When we probe at driver outputs +V0 and –V0 are not balanced. We are observing DC offset of around 150mV between them. We have 16 channels in our board and we are also observing DC offset across channels of around 400mV. Attached is the schematics of our design. We need your support for finding cause and solution to this problem.