Other Parts Discussed in Thread: LMP2022, OPA2277, LMP2021
Hello everyone,
I'm going to design the adaptation part of the ADC peripherical of F28M36. I want to use a two steps, one for high impedance input and the other step with a second order amplifier filter (with the necessary gain to adapt 5V signal to 3.3 V for the DSP).
I used to use OPA2277 amplifier for this applicattion and it works very well. However I have been looking for new amplifiers (time goes by and maybe there are cheaper amplifiers with same features). I found lmp2022 but I have some doubts.
I see that voltage supply is between 2.2 to 5.5 V and it has rail to rail output. I thought to supply it between 5V and 0V. It means that otuput voltage can be exactly 5V or 0V ? And, the same for the input? Sorry for these questions but I can't find this information on its datasheet (http://www.ti.com/lit/ds/symlink/lmp2022.pdf) .
In addition to these questions I would like to know your opinion for this amplifier for this kind of application. It will work such good as opa2277 amplifier?